Issue
Battery replacement for V53 processor card and 532 controller.
Environment
- V53
- 532 Controller
Cause
The battery supplied with the V53 processor board is dead and need replacement.
Resolution
The battery supplied with the V53 processor card and 532 controllers is rated at 70mAh.
Specification V53-BAT provides a battery rated at 150mAH.
The circuitry on both the V53 processor card and 532 controllers can handle this higher rated battery.