Getting MSMQ errors and Continuum fails to start

Issue

The issue is that MSMQ is not installed on the machine or the installation is corrupted. MSMQ is a windows component that needs to be installed for enhanced alarm delivery. The error displayed is "There appears to be a problem with the configuration of this system. Please check to make sure that you have correctly installed MSMQ."

Product Line

Andover Continuum

Environment

Windows OS

Cause

MSMQ not installed on PC.

Resolution

Install MSMQ from the Windows control panel/add remove programs/add remove windows components. Then reinstall Continuum.

NOTE: Have seen an few instances where uninstalling MSMQ from add/remove windows components and then allowing Continuum to install MSMQ resulted in a successful install of the MSMQ