Issue
All values in the Xenta 102-AX Plug-in are blank.
Product Line
TAC Vista
Environment
- Xenta 102-AX Plug-In
- LonMaker
Cause
If the Resource File Languages have become corrupted on your PC, then the plug-in will not know how to display the required data. Go to LonMaker > Network Properties > Resource File Languages.
If the only Language listed is "ENU," then the language files are corrupted. ENU is the default language and will display all data in the LNS environment -- plug-ins, browser, get values -- in an enumerated format that is not usable. Everything will continue to work, but monitoring data in the LNS environment and configuring ASCs via plug-ins will be impossible.
Resolution
Restore the Resource File Languages:
- Shut down LonMaker
- Go to http://www.lonmark.org/technical_resources/resource_files/
- Download LonMarkResourceFiles1300.exe
- Run the executable
- Restart LonMaker
- Check Network Properties again. US English should be listed and the plug-in should populate with data.
Note: There may be Beta versions 13.04 and 13.10 on this website. Do not use these LonMark resource files. The newer versions cause errors in the 102-AX plug-in. For more information see
.