How do I automatically backup the entire TAC I/NET Seven SQL database.

Issue

When only the MSDE version of I/NET Seven is installed there is no way to automatically backup the entire SQL Database at scheduled intervals.

Product Line

TAC I/NET

Environment

TAC I/NET Seven running on Windows XP using Microsoft MSDE SQL Server.

Cause

When only the MSDE version of I/NET Seven is installed there is no way to automatically backup the entire SQL Database at scheduled intervals.

Resolution

A batch file BackupInetDb.bat has been developed to allow users to create a Scheduled Task within Windows which launches the batch file with the appropriate command line switches. Click here to download the zip file which contains the BackupInetDb.bat and instructions on how to configure an automated backup.