Error Not enough space in RTI device

Issue

Error "Not enough space in RTI device"
 

Product Line

TAC Vista

Environment

  • Aladdin Privilege Administrator 2.01
  • Vista IV Licensing

Cause

Memory in PSU is corrupt.

Resolution

Run Dongleutil, a dongle reset utility software.
This utility resets the memory in the PSU that is connected to the PC.
You need to install the license file again after this operation.

This problem is usually seen when Inhouse PSU is used. In TAC Vista version 4.10 and later, it’s no longer necessary to install the engineering file when Inhouse PSU is in use. Just connect the PSU to the PC, and everything should work fine.