Issue
Xenta 121-FC SNVTs show up in LonMaker or NL220 but are missing in Vista
Environment
- Xenta 121-FC
- LonMaker/NL220
- Vista Workstation 4.5
- System Plug-in
Cause
A problem has occurred with the import of the controller into the Vista database.
Resolution
- In the Vista System Plug in, delete the controller from the TAC Network.
- In the LNS network tab, right click on the controller and disable it from being updated in the TAC Network.
- Update the TAC Vista Database
- Refresh the Folder View in Vista Workstation.
- Verify that the controller has been removed from Vista.
- In the Vista System Plug in, re-enable the controller to be updated in the TAC Network
- Move it back into its former location in the TAC Network
- Update the Vista Database a second time.
- Go to Vista Workstation, verify that the controller has returned and values are being properly displayed.