Issue
- Error number : 17040
Error description: Invalid format. (Subsystem: LNS, #40) - Any tab except "Status" has some strange values. Trying to view or edit some values results in this error.
Environment
- Xenta 102-AX Plug-in
- Xenta 104 Plug-in
- LonMaker
- NL220
Cause
A value inside the device has been set with an invalid value. It could be through an LNS browser, through an M/STAT or just through some glitch when setting a parameter.
Resolution
The device will need to be recommissioned using default values.
- CAUTION: Recommissioning a device with default values will erase any user defined configuration parameters. Record all important data for the box: duct area, airflow setpoints, operating parameters, etc.
- Right-click on the device in the LNS Management tool. In LonMaker, select Recommission. In NL220, select Repair.
- Choose "Manufacturer Defaults" for the initial values. Click OK.
- Launch the plug-in again. The values should now be able to be changed to the desired value.