Error: NS #31 lcaErrNsDeferConfigUpdatesMgmntMode

Issue

The requested service cannot be provided in the current management mode. 

Product Line

TAC Vista

Environment

NL220

ZBuilder

Xenta 121

Cause

Attempts to download a ZBuilder configuration to a Xenta 121 on a network that is not "attached."  This is the incorrect management mode to perform a download.

Resolution

Make sure the network status is onnet and attached.