Issue
The network subnet limit (currently 255) has been reached.
Environment
LNS
LonMaker
Vista
NL220
Cause
The network subnet limit (currently 255) has been reached.
Resolution
Run the LNS Database Recovery Wizard: If you are recovering through a PCC-10, PCLTA-10 or PCLTA-20, use the LonWorks Plug 'n Play Control Panel to select the NSI NI Application. Otherwise, error "NS #138 (Local interface is in the wrong state (unconfigured)" is reported, then "NS #67 system is not open)", then "LNS #55". Finally, the LNS Database Recovery Wizard only gives you the option to cancel the recovery.