Issue
There is a resource problem in the API or application.
Environment
- LonMaker
- NL220
- Vista
- LNS
- ZBuilder
Cause
This may be a compatibility issue observed when launching ZBuilder from LonMaker.
Resolution
Zbuilder may work many times after LonMaker is started, but eventually produce this error. Once the error was produced, it would reoccur every successive attempt. To launch Zbuilder successfully, LonMaker had to be restarted. When checking versions, it was discovered that there was ZBuilder 5.0.3 installed and ZBuilder part of the 5.1.0 ToolPack installed.