Issue
A query to an LNS collection object has been made using an invalid index number. The range of valid indices starts with 1 and ends with the current item count.
Environment
LonMaker
NL220
Vista
LNS
Cause
When launching the plug-in of a device.
Resolution
- In NL220, go to the "Plug-Ins" menu dropdown
- If the option exists, Verify that the option "Simple string command" is deactivated.
- If not, uncheck it and try to relaunch the plug-in.
*Note this option has been removed in more current versions of NL220, there may not be an option represented.