Issue
Microsoft TCP/IP Networking must be installed on your PC or a LNS #25, [DB #2524] error is reported.
Environment
LonMaker
NL220
Vista
LNS
Cause
Microsoft TCP/IP Networking must be installed on your PC .
Resolution
Microsoft TCP/IP Networking is normally installed during Windows operating system installation but it is an optional component if a network interface card (such as an Ethernet adapter) is not installed in the PC. Microsoft TCP/IP Networking is included on the Windows installation CD of all Windows operating systems that LNS 3 runs on. Depending upon the operating system that you are using (Windows XP, Windows 2000, or Windows 98), the Microsoft TCP/IP Networking component may be named slightly differently. Consult the Windows documentation for further information on how to install the Microsoft TCP/IP Networking component.
You can find the same information in the "Known Problems and Workarounds" section in LNS3.0 service pack's readme file.
See also Echelon support article 143