Error: LNS #25 lcaErrDatabase Database error. (Subsystem: LNS, #25)[DB#-2506]

Issue

"Database error. (Subsystem: LNS, #25)[DB#-2506]"

After clicking OK there may be another error:

"The global database is not open. (Subsystem: LNS, #64)".

When the Echelon LonMaker Design Manager opened, there is nothing in the Database Name field.

Product Line

TAC Vista

Environment

LonMaker
Vista
LNS

Cause

This error can occur when ports that the LNS Database is trying to use are already being used by other applications. The ports in question are 6001 and 6002.

Resolution

To check which application is using these ports, use the following DOS command:

netstat -bn

Once you know which application is using ports 6001 and 6002, shut that application down and relaunch LonMaker or your LNS-based application.

support.echelon.com and search for kb481