Issue
Under user admin in a Xenta server you can change the content of the 3 frames that the user sees when logging in.
If the user have changed the default frames for the root user in a Xenta server so that the tree navigation is not available you can't navigate back to user admin to reset the frames.
Environment
- TAC Xenta Server
- Xenta 511, 527, 555, 701, 711, 721, 731, 913
Cause
User have changed the frames so that the menu tree is no longer available
Resolution
- Log on to the Xenta server with the root account.
- Type in https://xx.xx.xx.xx/wm/useradmin/ in the IE address field.
- This takes you directly to the useradmin page.
- Click on the root user.
- Under Frame Settings click on Use Default for the Menu frame.