Issue
Is the ICI editor and associated BIN files still available.
Environment
I/Net Seven all revisions.
7797 ICI all firmware revisions connecting to a third party device.
Cause
It is not clearly defined in the documentation the location of the ICI Editor and associate BIN files.
Resolution
The ICI Editor is part of the I/NET install CD, the application is found under the folder name ICI-CD.
The associated BIN files for these devices are also located on the I/NET CD under the folder name SUPPORT\BINS.