Error: LNS, #148 lcaErrXDriverNoSuchProfile

Issue

The xDriver profile selected does not exist, or the xDriver connection broker is not currently running.

Product Line

TAC Vista

Environment

LNS
NL220
LonMaker
Vista

Cause

Make sure that the profile you are using exists, and that the xDriver connection broker service has been started if you encounter this error.

Resolution

For more information on the xDriver connection broker, see the OpenLDV Programmer’s Guide, xDriver Supplement.

http://www.echelon.com/support/documentation/manuals/devtools/078-0275-01C.pdf