Issue
An error is received, comm port is not enabled when trying to apply the 2nd generation xdriver file to comm2 on a BCX.
Environment
- Continuum 1.9x
- BCX4040
- Xdriver
Cause
Typically comm2 is set to mstp. Trying to apply the Xdriver file to the comm port thinks it already has the port applied and renders the error.
Resolution
- Pull the battery connection
- Power off the controller which sets the port to autoset
- Power up the controller
- Set comm2 to xdriver and apply the file and no error is received
- -If this still doesn't work then update the firmware, it may resolve the issue
If this does not resolve the issue try Clearing Database Backup from the controllers webpage and reload.