Issue
How to allocate a range for individuals on an I/NET system.
Environment
I/NET Seven
Cause
Individual Needs to be added to I/NET Seven
Resolution
Select the Individuals tab from Access/Individuals and choose the Tenant that the individuals are being added to. On the bottom of the editor is a button called Allocate Range, select this and when the editor comes up and put the number that you want to start from as well as the number of individuals that is being added and click on the Okay button. The Individuals will be added immediately to the system and they you can make necessary changes to each as deemed fit.