Issue
- Various error when trying to login, cant open graphics
Environment
- Vista webstation
Cause
Java errors i.e. When opening graphic error "Error: Click for detail" or Dynamic mode not functioning.
Resolution
Dynamic picture not working are most likely caused by wrong Java version. Vista 5.1.4 uses Java 1.6-17 but installing this version afterwards might causes other problem like "Error: Click for detail (various java code errors). This can be resolved by reinstalling the webserver again or check for the following.
-
IIS use the wrong version of .NET.
- - Go to administrator tool and choose Internet information services.
- - Choose Web sites then Default Web Site
- - Right click on Webstation and choose properties
- - Go to the ASP.NET tab and make sure the version specified are 2.0....
-
Address used HTTP://IP/defaultpage.aspx when it should be using HTTP://IP/webstation/defaultpage.aspx
- - Go to same path as above but instead of right clicking the Webstation right click on the tree above "Default Web Site" and choose properties.
- - Go to the tab Home directory and check local path it should be directed to wwwroot (see attached) Then write in the address HTTP://IP/webstation/ (might work if you try directly)
- There have always been problem in which order you install programs, it has been noticed that sometimes java needs to be installed before webstation since webstation tries to reach components in java that do not exist else. So a try would also be to reinstall webstation now when the new Java version are already installed.