Issue
Error "Continuum is already running" while trying to start Continuum.
Environment
Continuum 1.91
Windows XPsp3
Cause
Continuum was not gracefully shut down, which left some services running.
Resolution
- Reboot PC which will terminate all services or use Continuumprocesses.exe in the Continuum folder
- If this is an upgrade ensure that the database has been updated prior to starting Cyber with the transferred database
- Make sure the Workstation initialization was completed prior to starting Cyber.