I/NET CD Key and software revision

Issue

Which CD Keys can be used with which version of I/NET Seven Software?

Product Line

TAC I/NET

Environment

I/NET Seven - all revisions.

Cause

Need to know which CD Key can be used with which version of I/NET CD

Resolution

The I/NET CD Key is comprised of

  • User Name
  • Site Name
  • Key; provided in the format XXXX-XXXX-XXXX-XXXX-XXXX.

The key provided above is a 20 character key, segregated into five 4 character sets.  The second set of four characters (shown in bold and underlined above) and using the table below, will help identify which version of I/NET Seven Software works with which CD-Key:

 

I/NET Seven Version

CD Key

I/NET Seven 1.xx

XXXX-D71R-XXXX-XXXX-XXXX

I/NET Seven 2.00 to 2.31 (Excluding 2.30)

XXXX-E71R-XXXX-XXXX-XXXX

I/NET Seven 2.30 (Only)

XXXX-F71R-XXXX-XXXX-XXXX

I/NET Seven 2.4x

XXXX-F71R-XXXX-XXXX-XXXX