Issue
How to use two door readers on one input.
Environment
Continuum Access Controllers
- AC1
- AC1Plus
- ACX78x
- ACX57xx
- 9702
Cause
Trying to use two door readers on the same input without interface to handle two signals.
Resolution
KIM board was designed to handle two door readers on the same input.
Search customer Iportal for "KIM" for part number
KIM 01-0009-059