How do you locate error messages in Cyberstation?

Issue

At times errors either pop up in Cyberstation or you may see an error in the error listview.

Product Line

Andover Continuum

Environment

Continuum

All operating systems supported by Continuum

Cause

When troubleshooting, errors appear in Cyberstation or in the error listview.

Resolution

With Continuum running and with the focus on the main Continuum screen or Continuum Explorer, press F1 to bring up help

  1. Select index
  2. Type in ‘error’
  3. Select Error Messages, Cyberstation
  4. This displays a list of some of the error messages that may come up in Cyberstation.

This is not a comprehensive list and it doesn’t provide solutions, but gives an initial idea of what is happening for troubleshooting.