Issue
Save error
There is no file associated with the object
It is possible to create the TGML object in TAC Vista and right click and edit it but not to save the changes.
Environment
- TAC Vista 5 Workstation
- TGML Graphic Editor
Cause
It is not possible to save any TGML graphic in a TAC Vista folder that has a ":" (colon) in the name.
Resolution
Change the name of the folder to not include a ":" (colon).