Issue
- Changes made in TAC vista workstation are not saved in TAC Menta.
- Change of alarm texts made in TAC Vista workstation are not saved in TAC Menta
- Change of value of a PVR block made in TAC Vista workstation is not saved in TAC Vista.
Environment
TAC Vista 5.1
Cause
In TAC Vista workstation it is possible to type in texts in the description field that are longer then TAC Menta allows.
If you do this no changes made to that signal (block) done from TAC Vista workstation will be saved in the TAC Menta file
Resolution
Edit the Description for the block so that it is 41 characters of less.