Issue
Can controllers running with FTT Lon communicate with controllers running 485 Lon?
Environment
NC1 - CX9900
NC2 - CX9980
Cause
Question about whether the type of LON bus (FTT/485) affects communications at the IP level
Resolution
The NC1/NC2 and its IOU modules must be of the same type (FTT/485) but this does not effect communications between the NC1/NC2s at the IP level