Issue
Is there a Fiber Optic option for the Continuum IO bus
Environment
Continuum CyberStation
Netcontroller I
Netcontroller 2
Cause
Need to run IO bus between buildings
Resolution
There is no Fiber Optic option for the Continuum IO bus. The only option would be to put individual Netcontrollers in each building.