Issue
Upgrade of Continuum displaying error "C:\program files\continuum\userprofiles\xpress.mnu" unable to locate
Environment
Continuum Cyberstation
Cause
Upgrade of Continuum software was unable to located a custom menu file. Suspected file was not in specified location.
Resolution
Once logged into Continuum.
- Edit workstation
- Select Preferences tab
- Select "The File name of the menu"
- Browse for location of the Custom *.mnu OR select default location "C:\program files\continuum\userprofiles\Continuum.mnu"
Note: if the patch on the previous installation was non-standard, then save off a different Continuum.mnu, point all the buttons to the new path, save it and then point all the Cybers to the new Continuum.mnu