Temperature inputs not reading the correct value

Issue

Temperature inputs not reading the correct values

Product Line

Andover Continuum, Other

Environment

  • Cyberstation
  • IOUs
  • Controller

Cause

Bad input

Bad controller

Bad sensor

Resolution

Replace sensor with a 10k ohm resistor.  Temperature input should read roughly 77°F or 25°C.  If it does then the problem is with the sensor.  If it does not then the problem is either with the input board or that particular input itself.