Issue
Is IPv6 supported with Continuum Netcontrollers?
Product Line
Andover Continuum
Environment
BCX 4040
BCX 9640
9680
ACX57xx
Cause
IPv6 compatibility with Continuum Netcontrollers
Resolution
As of today, 3/21/2013, Continuum controllers do not support IPv6. There are no plans at this time to implement IPv6 into Continuum controllers.