Issue
Is a Vista license necessary for I/NET Host tool features or is the I/NET CD key sufficient?
What is the difference in the I/NET Integrated and I/NET Security licenses?
Environment
Vista Server
I/NET Host Tool
Cause
The I/NET Host tool requires a Vista license file to run. Certain editors and features in the I/NET Host Tool are common to both the Integrated and Security license. Some features are specific to the Integrated or Security license. To have all of the features purchase of both licenses is necessary.
AMT is not included with the I/NET host tool product as Vista is expected to handle alarms messages and transactions
Common Features
-
System features
- Change password
- Connect/Disconnect
- Logon/Logoff
- Quit
- Work offline
-
Host features
- Host configuration editor
- Host password editor
- Host phone numbers editor
- Host software restore editor
- Netcon function editor
- Network configuration editor
- System view
-
Tap features
- Host, link, and site tap configuration
- Site tap remote configuration
- Site tap save/restore
-
Controller features
- 7720 configuration editor
- Action messages summary
- Alarm extension editor
- Calculation editor
- Control description editor
- Conversion coefficient editor
- DCU configuration editor
- DCU save editor
- DCU restore editor
- DCU password editor
- DPU configuration editor
- Engineering units editor
- Event extension editor
- Event sequences summary
- I1/I2 state parameters editor
- Lighting circuits editor
- Lighting zones editor
- LCD page definition editor
- Lookup table editor
- MCU configuration editor
- MR configuration editor
- Resident point editor
- Special days editor
- State descriptions editor
- Time schedule extension editor
- Trend extension editor
- Trend plot view dialog
-
Summaries
- Configuration summary
- Controller summary
- Disabled points summary
- Off-normal points summary
-
Reporting features
- SevenReports (operates in view-only mode if no I/NET CD key is installed)
I/NET Integrated only
-
Controller features
- Consumption extension editor
- DDC modules summary
- Demand control extension editor
- MR DDC summary
- Override billing equipment mapping editor
- Override billing extension editor
- Override billing parameter editor
- Runtime extension editor
- Temperature control extension editor
- Unitary control configuration editor
- Unitary control extension editor
I/NET Security only
-
Controller access features
- Elevator extension editor
- DCU AIC editor
- Door extension editor
- Personnel schedules
- SCU parameters editor
-
Host access features
- Access control options editor
- Access control wizard
- AIC editor
- Door extension editor
- Groups editor
- Individuals editor
- Key translation editor
- Personnel schedules
- Pin generation dialog
- Recycle bin
- SCU editor
- Tenant editor
- User search
-
Summaries
- Door tenant summary
Resolution
Purchase of an I/NET Host Tool license is necessary for the integration with Vista Workstation to function.
Use the feature list to determine if only one license or both licenses are required by the customer.
Attached is the PA for all the required software Here