An Unknown Error is received DNWacserverFactory/WACServerFactory.soap when accessing webclient 1.9x pinpoint using Windows Server 2008

Issue

Instructions listed in the webclient installation guide have been followed.

Accessing Webclient pinpoint from any browser, the following error occurs when Webclient is installed on Windows Server 2008

"Unknown Error.
Server:http://ServerNameDNWACserverFactory/WACSERVER
Factory.soap"

Product Line

Andover Continuum

Environment

Webclient

Windows Server 2008

Cause

The 1.92 Webclient installation instructions do no include all the instructions to configure Webclient Pinpoint for Windows Server 2008. This has been corrected in 1.93.

Resolution

The 1.92 Webclient installation instructions do not include all the steps needed to configure Webclient Pinpoint for use on Windows Server 2008. The complete set of instructions are included in the 1.93 release of Webclient.

Click here for the 1.93 instructions for Server 2008

Click here for a sample web.config file