I/NET third party password (INetThirdParty) login not working with I/NET Seven 2.40 and above

Issue

Unable to login in to the I/NET SQL database using the default password for login name  INetThirdParty.

Seven ODBC Settings can not be changed using the INetThirdParty login, receive 'SQL Login Error: 18456'

What is the I/NET third party password?

Product Line

TAC I/NET

Environment

Windows XP, Windows Server 2003, Windows 7

I/NET Seven 2.40 and above

Cause

The I/NET Seven INetThirdParty password needed to comply with security requirements for Windows 7 and SQL 2008.

Resolution

The INetThirdParty password is now PassInetDb3p_SE (case sensitive). for  I/NET Seven 2.40 and above

For Inet 2.31 and below its PassInetDb3p