Issue
Alarms not showing up in the alarm list.
Environment
TAC Vista Workstation
TAC Vista Server
Cause
- The alarm could be disabled.
- The alarm might have priority 0 (info).
- There might be a filter in place in the alarm list.
Resolution
- The alarm could be disabled, in workstation go to View > Disabled alarms to see the list and enable again.
- The alarm might have priority 0 (info). No Alarms with priority 0 is shown in the alarm list.
- There might be a filter in place in the alarm list, in the alarm view you are using right click and select filter to check this. A good practice is to set the "Date and Time" tab settings to reflect "Tripped " and "Last change" to show all alarms. This is done by checking the four checkboxes for "First alarm" and "Last alarm" allowing all alarms to be viewed.