Issue
Values for a MODBus address are not coming in while using the MODbus RTU X-Driver
Environment
Controller
MODBus
X-Driver
Cause
The data type configured in the X-Driver point did not match the data type from the address on the third party device
Resolution
Review the data type from the third party documentation and configure the X-Driver point with the correct data type