Has Bomgar been tested with Continuum and is it supported

Issue

Has Bomgar been tested with Continuum and is it supported

Product Line

Andover Continuum

Environment

Continuum Cyberstation

Bomgar

Cause

Compatibility of Bomgar remote desktop software with Continuum

Resolution

Bomgar has not been tested with Continuum and therefore is not supported.

NOTE: This is not to say that it will not work. It appears to be a remote desktop type of software. The issue with remote desktops, is that most will work for accessing a system. But where things go wrong are installations of software over remote connections. Also there can be video and graphic issues with remote desktop applications.