Created a digital schedule in an AS-B folder and it never changed the value of the digital value

Issue

Created a digital schedule in an AS-B folder and it never changed the value of the digital value

Product Line

SmartStruxure Solution

Environment

  • StruxureWare Building Operation
  • Time Schedule
  • AS-B

Cause

Digital value bound to a digital schedule failed to change the value when the configured schedules time daily event changed

Resolution

Configure Date and Time of AS-B:

  1. Click on the AS in workstation
  2. Go to the Date & Time tab
  3. Set the proper time zone and save the changes.
  4. Manually adjust the time if needed and save the changes again.