Default IP address for BCX, ACX57xx, CX9702 & Netcontroller II

Issue

What is the default IP address for BCX, ACX57xx, CX9702 & Netcontroller II?

Product Line

Andover Continuum

Environment

Controller

Netcontroller II (9680)

BCX

ACX57xx

CX9702

Cause

Default IP address for BCX, ACX57xx, CX9702 & Netcontroller II

Resolution

The default IP address for all these controller types is 169.254.1.1, the subnet is 255.255.0.0, and the gateway is 169.254.0.0.