What are the default passwords for a MicroNet Touchscreen?

Issue

What are the default passwords for a MicroNet Touchscreen?

Product Line

Satchwell MicroNet, Other

Environment

MicroNet Touchscreen controllers

Cause

Access level

Resolution

Read only: -      1234

Read/Write: -   4321

Super User: -    1024

ACK Alarm: -  2513

It is worth noting that these passwords can be changed when programming.

If you connect to the Touchscreen using VisiSat software you can identify the passwords under the properties of the Touchscreen.