Issue
Viconics Stats will not come on line.
Environment
- Continuum 1.XX
- Windows XP, 2003
- Viconics Stat
Cause
Viconics Comm address set to 50
BACnet Max Master set to low, Set to 32.
Resolution
- Open Continuum Explorer
- Expand Bac Net devices
- Edit the BCX ( Bac net view)
- Change the BACnet Max master value