Issue
When Acknowledging an Alarm from one workstation it is not making it to all workstations.
Environment
CyberStation
Alarm
Cause
The workstation that was not receiving the Acknowledgement had two network cards in it.
Resolution
Remove the second network card from the PC. Pleas note Continuum only supports one network card in a CyberStation.