Are 64-bit operating systems supported on the Andover Continuum product line?

Issue

Are 64-bit operating systems supported on the Andover Continuum product line?

Product Line

Andover Continuum

Environment

CyberStation

webClient

Cause

Are 64-bit operating systems supported on the Andover Continuum product line?

Resolution

  1. For all machines with CyberStation or webClient software installed, only operating systems running in 32-bit environments are supported. 64-bit environments are not supported. (The previous comment applies to releases prior to 1.94. 1.94 was released to support 64 bit OSs)
  2. However for the Database Server on a LAN system where no Cyberstation or webClient software is installed, a 64 bit version of Windows Server 2008 (SP2) or Windows Server 2008 R2 may be used on systems running V1.92 and above. These will also require Microsoft SQL 2008 running in 64 bit mode.