Remote Client options is missing from Workstation Options in I/NET 2.40 I/NET Configuration Profile.

Issue

Remote Client Option is missing from Workstation Options in I/NET 2.40 I/NET Configuration Profile.

Product Line

TAC I/NET

Environment

I/NET

Cause

The I/O Server must be shut down in order to make this change to an I/NET Configuration Profile.

Resolution

  1. Close the Configuration Profile Editor
  2. Exit I/NET
  3. Shut Down the I/O server
  4. From the Start Menu, Open I/NET Configuration Profile Editor
  5. You should now be able to set the computer to Remote Client