Issue
An InfinityProgram is setting an output point but the point does not change value, the program is enabled and running.
Environment
- CyberStation
- CX9900
- CX9680
- ACX57xx
- All infinet and i2 devices
Cause
This issue may be caused by a number of reasons:
- The InfinityOutput object is disabled.
- The InfinityOutput object is manually overridden.
- A second program that executes later in the firing order is setting the output object.
Resolution
- Enable the InfinityOutput object.
- Return the output override switch to the 'Auto' position.
- Solve the contention between programs.