Issue
Adding area(s) to multiple personnel objects in one operation
Environment
CyberStation
Cause
Need to add area(s) to multiple personnel objects in one shot
Resolution
- In the Continuum Explorer select the folder that contains the personnel object.
- In the right pane select the personnel objects you want to add the area(s) to, you can select ‘Edit\Select All’ from the pull down menu or use a combination of the Shift/Ctrl key with the left button mouse click to multi select.
- Right click on one of the selected Personnel objects and select ‘Add Areas…’ from the context menu.
- In the ‘Area’ window you can select one or more areas to assign.