Issue
How do I determine whether a Valid Access event took place at the entry or exit side of the door from within a PE program?
Environment
- CyberStation
- CX9702
- CX9900
- CX968x
- ACX57xx
- ACX7xx
- IOU Modules AC1, AC1A, AC1Plus
Cause
Need a way to determine which side of a dual reader door a valid access event has taken place.
Resolution
Compare the door’s TimeEntered attribute to the TimeExited attribute, if TimeEntered > TimeExited then the event took place at the entry side of the door, otherwise it took place at the exit side.
The same technique can be used for Invalid Attempt events using the door’s InvalidEntryTime and InvalidExitTime attributes