Issue
Using the "TemplateName" and "TemplateAlias" attributes in a ListView, does not show the attached Personnel Template.
Environment
Continuum Cyberstation
Cause
Not using the attribute "RefTemplate" to view attached Personnel Templates.
Resolution
Use the attribute "RefTemplate". This is the Personnel's referenced template and is the field used to link to the template.
- Open the Personnel ListView where you want to view the attached template.
- Select View-> ListView Configuration.
- On the columns tab select "Add Column".
- Select attribute field and from the drop down list select "RefTemplate"
- Save Listview and re-run. It now shows the attached templates in the RefTemplate field.