Issue
When a Vista trend is added manually or using the Trend Wizard on completion of the process the error massage "Invalid Entrance" is displayed.
Environment
Vista 5.0.3 and Windows Server 2003.
Vista Master and Slave configuration.
Cause
The trend is being added in the Master Vista Server and the point is in a Slave Vista database.
Resolution
To add a Vista trend log of a point residing in a Slave Vista sever use the following steps.
- Log onto the Vista Slave server.
- Add a new or use an existing directory (ensure this folder is visible to the Vista Master Server) that has been created on the Vista Slave.
- Add your Vista trend either using the trend wizard or manually.