Issue
When attempting LonWorks communications in WorkPlace Tech, the following error message is seen.
"Failed to get communications type, using LonWorks as default"
Product Line
TAC I/A Series
Environment
WorkPlace Tech 5.7.x
Echelon U10 USB LON Network Interface (part number ECH-75010) – TP/FT-10 Channel
Cause
WorkPlace Tech LonWorks communications is not properly initialised.
Resolution
Re-initialise WorkPlace Tech LonWorks communications.
- In WorkPlace Tech, go to 'Tools' > 'Configure Communication'.
- Change the communications type to 'BACnet' and click 'OK'.
- Open up 'Configure Communication' again and change the communications type back to 'LonWorks'. This should re-initialise the LonWorks communications.