Issue
In XPSI 4.1 Terminal Mode, there is a noticeable delay in the action of the “Escape” key when backing out of a Current Status or VEO group display screen.
Environment
XPSI rev 4.1, Windows XP SP3, Windows Vista Pro, Network 8000 GCM, Network 8000 LCM
Cause
Serial communications are slower with the Microsoft port controls used with XPSI version 4.1.
Resolution
The “Escape” key will work, it just takes a few seconds longer in version 4.1 than it did in earlier versions, such as 3.13.